Other Parts Discussed in Thread: TMDSEMU110-U, UNIFLASH
Tool/software: Code Composer Studio
I purchased a new XDS110 (TMDSEMU110-U) for a friend. After connecting it to the target board and try to upload code through CCS, CCS prompts to update firmware for XDS110. So, I clicked "Update" button to proceed. But the dialog hangs. I found I have to unplug the USB cable to release it. Then, I try to update firmware on console, but got error DFU_ERR_UNSUPPORTED (-5). I have tried many times under both Windows and macOS. The result is the same. Here is the console output. Does anyone have idea?
xdsdfu -m
USB Device Firmware Upgrade Utility
Copyright (c) 2008-2015 Texas Instruments Incorporated. All rights reserved.
Scanning USB buses for supported XDS110 devices...
<<<< Device 0 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Probe with CMSIS-DAP
Version: 2.3.0.5
Manufacturer: Texas Instruments
Serial Num: 00000000
Mode: Runtime
Switching device into DFU mode.
xdsdfu -f firmware.bin -r
USB Device Firmware Upgrade Utility
Copyright (c) 2008-2015 Texas Instruments Incorporated. All rights reserved.
Scanning USB buses for supported XDS110 devices...
Downloading boot_loader.bin to device...
Error DFU_ERR_UNSUPPORTED (-5) reported during file download