Part Number: TMS320DM642
Tool/software: Code Composer Studio
Hello.
I have got a project made for tms320dm642 in ccs3.0 or ccs3.1. I do not use the dsk board for dm642 we have our own board created by our company.
I need to open the project, recompile it and load the out-file back into tms320dm642.
I have got ccs3.3. I managed to open the project and recompile it, so the out-file is created. But when I'm trying to load it into the dsp dm642- the IDE tells me about the mistmatch of the target type (picture 1).
On my dsp I tried to use EVMDM642.gel file and DSP64xxplus.gel file (picture 2) - but I have got the same result.
I know that my project was created in ccs 3.0 or ccs3.1 and the result out-file I can load into the dm642 processor using my ccs3.3, but I can't make good recompiled out-file, that can be loaded into the dm642 proceccor.
Please tell me what can be the reason of the problem, and how can I solve it? May be I need the earlier version ccs 3.0 or 3.1? So where I can download it - to have the oppotunity to create a suitable good out-file that can be loaded into my dsp dm642?

Thank you.
Liashchonak Ilya
newmail36@mail.ru
+375336262533