Hello ,
when i am trying to save a file in CCS V4 I am getting Cp1252 problem not able to save change text to Cp1252 encoding.
I tried changing to UTF-8 or using other options but it does not help, any suggestions anyone.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello ,
when i am trying to save a file in CCS V4 I am getting Cp1252 problem not able to save change text to Cp1252 encoding.
I tried changing to UTF-8 or using other options but it does not help, any suggestions anyone.
no, i do not have any special characters in the source file. Yes i copied the code from the CCS V4 to a notepad file and word fileand was able to save them.
Thanks for attaching the file. I see the issue now. There are some special characters in there that is causing the problem. I'm not sure which one it is. I think it is in the comments somewhere. Anyway, if I cut and paste into notepad and then save the file in there, and then add the file to the project, it seems ok since notepad will convert the file when you save it.