CCS4.1.13.0038, DSP/BIOS 6
I want to use the same RTSC Configuration in two different CCS Projects.
I thought the way to do this was to create one project with a new RTSC Configuration Project which also automatically creates a referernce to the new RTSC Configuration Project. Then create another project and check "Reference an existing RTSC Configuration project" on the "Referenced RTSC Configuration" page then select the previous Configuration Project.
But then I ran across FAQ-080729-5 which reccomends creating a separate Configuration-only Project, then referenceing that project in the Additional Project Settings page. I tried to find documentation on exactly what "inter-project depoenicies" really means but all I got was "Creating a New Project".
Now I am -really- confused. Which is it? Or does it matter? What is "inter-project depoenicies"?