This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am writing code for the C64x Core. I found it very useful to use an implementation of the intrisincs for PC host on which I can develope and Debug my code before Working on the DSP. My team was using an old implementation we found in an article from TI. in recent time i found the following link:
https://www-a.ti.com/downloads/sds_support/applications_packages/c_intrinsics_host_port/index.htm
where one can find a new software package to enablecode development on a PC Host. while using the software i found that the implementation of _mpylir is not bit exact with the results i get on the DSP. for example: _mpylir(-1, 2147467264) will return a value of -65536 on the PC while on the DSP, you will get -65535. similarly _mpylir(-1, 2147434496) will return -65535 on PC and -65534 on DSP.
the TI support have directed me here to find an answer. for now I am using a mix of the old code and the new one.
is there a new version planned for this software package ?
moshe haim said:is there a new version planned for this software package ?
This particular bug has already been reported and fixed in internal development versions. Since it is short, I'll publish the corrected version of these intrinsics here. Note _mpyhir had to be fixed as well.
int32 _mpylir(int32 a, int32 b)
{
union reg32 a32;
union reg64 a64, b64, y64;
a32.x1 = a;
if ((a32.x2.lo == MIN_INT16) && (b == MIN_INT32))
{
CSR |= DSP_CSR_SAT;
return MAX_INT32;
}
a64.x1_ll = a32.x2.lo;
b64.x1_ll = b;
y64.x1_ll = (a64.x1_ll * b64.x1_ll + 0x4000) >> 15;
return y64.x2.lo;
}
int32 _mpyhir(int32 a, int32 b)
{
union reg32 a32;
union reg64 a64, b64, y64;
a32.x1 = a;
if ((a32.x2.hi == MIN_INT16) && (b == MIN_INT32))
{
CSR |= DSP_CSR_SAT;
return MAX_INT32;
}
a64.x1_ll = a32.x2.hi;
b64.x1_ll = b;
y64.x1_ll = (a64.x1_ll * b64.x1_ll + 0x4000) >> 15;
return y64.x2.lo;
}
I hope this is a practical workaround for now.
Thanks and regards,
-George