This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I installed ccs v3.3 in c drive and installed spectrum digital driver release 3.03.30(25 june 2009) in c\ccs3.3 . when checked in the ccs set up platform ''xds510 usb emulator ''is not shown. how could i add the emulator to platform?
Hai,
im using TMS3F28335 and TMS320F2810, former is the acquisition DSP while later is the signal generation dsp. a reference of the transmitted signal is stored in 28335 tx ref signal is given to internal ADC of 28335, after conversion the results from adc result registers are moved to a DMA buffer whose size is 2000. now i want to see the CCS graph of the signal stored in DMA buffer, my code flow is like the following,there are two handshake signal to communicate between dsps , after their communication , adc conversion starts by setting AdcRegs.ADCTRL2.bit.SOC_SEQ1 =1, then dma channel is enabled by setting DmaRegs.CH1.CONTROL.bit.RUN = 1. does the dma buffer flag set after filling the dma buffer? is the tx ref signal visible in CCS graph only when dma buffer is filled completely? do we need to make .CONTROL.bit.RUN = 0?