This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Below is the given default setting for linker cmd file. I am using a similar .cmd file to link the example code: Dotp4clasm.
Then in the disassembler window, I found a lot of data mistranslated into instructions, like 0x00040003 end up to be NOP.
Also the section that contain data is named .far in the .map file. Anyone can explain why?I have read the data sheet spur186.
No such information.
What is the use of each section please? especially .far .stack .switch, etc.
Thank you very much.
Da
MEMORY
{
RAM : origin = 0x00000001, length = 0xFFFFFFFE
}
SECTIONS
{
.text : ALIGN(32) {} > RAM
.const : ALIGN(8) {} > RAM
.data : ALIGN(8) {} > RAM
.bss : ALIGN(8) {} > RAM
.cinit : ALIGN(4) {} > RAM ; cflag option only
.pinit : ALIGN(4) {} > RAM ; cflag option only
.stack : ALIGN(8) {} > RAM ; cflag option only
.far : ALIGN(8) {} > RAM ; cflag option only
.sysmem: ALIGN(8) {} > RAM ; cflag option only
.switch: ALIGN(4) {} > RAM ; cflag option only
.cio : ALIGN(4) {} > RAM ; cflag option only
da cheng said:Also the section that contain data is named .far in the .map file. Anyone can explain why?I have read the data sheet spur186.
No such information.
What is the use of each section please? especially .far .stack .switch, etc.
Thank you very much.
SPRU187 also has some more information on the sections. See section 5.4.5.
http://focus.ti.com/lit/ug/spru187o/spru187o.pdf
ki
The .far section should not contain any initialized content. No code or data. It is used to merely reserve space in memory. Forget about your disassembly problem for the moment. Let's focus on why your .far section contains a NOP (or whatever). Look in your .map file. This file is created by the linker with the -m option. The .far section in a normal map file looks something like this.
.far 0 000099a0 00000350 UNINITIALIZED
000099a0 00000194 rts6200.lib : defs.obj (.far)
00009b34 000000d0 : trgdrv.obj (.far)
00009c04 000000cc : lowlev.obj (.far)
00009cd0 0000000c : exit.obj (.far)
00009cdc 00000008 : _lock.obj (.far)
00009ce4 00000008 : memory.obj (.far)
00009cec 00000004 : fopen.obj (.far)
I bet your map file looks different. Please post that part of your map file here.
Thanks and regards,
-George
Hello,
Following is my .far part in .map file:
.far 0 80007a60 00000988 UNINITIALIZED
80007a60 00000374 rts6700.lib : defs.obj (.far)
80007dd4 00000190 : _printfi.obj (.far)
80007f64 00000190 : fcvt.obj (.far)
800080f4 0000011c : lowlev.obj (.far)
80008210 000000d0 : trgdrv.obj (.far)
800082e0 0000008c : exit.obj (.far)
8000836c 00000064 : ecvt.obj (.far)
800083d0 00000008 : _lock.obj (.far)
800083d8 00000008 : memory.obj (.far)
800083e0 00000008 dotp4clasm.obj (.far)
Then there is the program part:
80007920 dotp4clasmfunc:
80007920 0018105A MV.L2X A6,B0
80007924 0290105B MV.L2X A4,B5
80007928 01901058 || MV.L1X B4,A3
8000792C 020000F8 ZERO.L1 A4
80007930 021436C6 LDH.D2T2 *B5++[0x1],B4 // this statement access the data around address 800083e2
80007934 00006000 NOP 4
80007938 028C3644 LDH.D1T1 *A3++[0x1],A5
8000793C 00006000 NOP 4
80007940 0290BC80 MPY.M1X A5,B4,A5
80007944 00000000 NOP
80007948 0210A078 ADD.L1 A5,A4,A4
8000794C 0003E05A SUB.L2 B0,1,B0
80007950 2FFFFE10 [ B0] B.S1 0x80007930
80007954 00008000 NOP 5
80007958 000C0362 B.S2 B3
8000795C 00008000 NOP 5
Then here is the data part(.far part in disassembly window):
The bold data{2,3,4,5} is defined by me. They are mistranslated.
800083B2 7C4B7FFF .word 0x7c4b7fff
800083B6 7C477FFF .word 0x7c477fff
800083BA 7C437FFF .word 0x7c437fff
800083BE 7C3F7FFF .word 0x7c3f7fff
800083C2 7C3B7FFF .word 0x7c3b7fff
800083C6 7C377FFF .word 0x7c377fff
800083CA 7C337FFF .word 0x7c337fff
800083CE 79A07FFF .word 0x79a07fff
800083D2 79A08000 || [!B2] NOP 5
800083D6 04008000 NOP 5
800083DA 87E80000 [ A1] NOP
800083DE 00028000 .word 0x00028000
800083E2 00040003 NOP
800083E6 7C170005 .word 0x7c170005
800083EA 7C137FFF .word 0x7c137fff
800083EE 7C0F7FFF .word 0x7c0f7fff
800083F2 7C0B7FFF .word 0x7c0b7fff
800083F6 7C077FFF .word 0x7c077fff
800083FA 7C037FFF .word 0x7c037fff