Part Number: 66AK2H12
Tool/software: Code Composer Studio
Trying to debug object on the ARM is giving me fits.
Using: CCS 7.3, GNU v4.9.3, XDCtools 3.32.2.25
I posted similar a while ago. Ref: https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/629959
I get different results when trying to view objects in the Expression window. For some objects the Type is displayed correctly but the value will have ??? marks after the address and when expended the value column says "invalid member name in macro". What does that mean?
Other objects are displayed with a type void * and when I try to expand those the Value column gives me "cannot load from non-primitive location".
This is significantly impacting my ability to debug. I don't understand what the conditions are that cause the above two things to happen. The code works as designed as far as I can tell.
It seems like it has something to do with having base classes with virtual members. Even a virtual destructor. If I remove all virtual functions than the debugger seems to allow me to view the object. I'm loathed to dispense with the use of virtuals but for the trade off of being able to debug I've started doing just that.
Can anyone offer any guidelines or suggestions? Is there something I need to configure to properly debug? Some code structure I should be avoiding?