Other Parts Discussed in Thread: TM4C1294NCPDT, TM4C123AH6PM
Tool/software: Code Composer Studio
CCS is 7.3.0.00019 Running in Win7
In our project, we need to add a Static Library which happens to be in the same workspace.
For resolving the headers, what we do is to go to CCS Build -> ARM Compiler -> Include Options -> Add dir to #include serach path
The desired directory is NOT showing up on the Includes folder of the project explorer. And a different library is showing up there with a purple folder icon, and we can't find a reference to this "undesired" folder anywhere!
This *TM4C123* library IS NOT being included by anything project parameter that we can think of!
Rebuilds, clean, properties/index/rebuild, erasing the project sub-folders that are re-criated by CCS, none of these have worked.
Any hints?
Regards
Bruno