Part Number: CC1350
Tool/software: Code Composer Studio
Hello,
I am designing my own PCB with CC1350 and I am planning to use segger j-link emulator as the debugger. I am testing its usage and functionality using CC1350 LP and CCS IDE.
I have wired the JTAG connector to appropriate pins on the LP since i dont have any kind of converter to put between the 10-pin connector on-board and the 20 pin connector that came with the emulator.
My questions -
1. What should be the jumper position for VSENSE? I tried placing it on XDS, external power and completely removing it; all 3 positions gave the same error.
2. What should I do with the pins on the 20 pin connector that I am not using (for example, TRST, RTCK and VCC_Optional)
3. I followed the instruction given here - 
And I am getting errors - firstly it shows in CCS debugger mode that Segger J_Link Emulator is Disconnected: Unknow
When I try to connect using JLink Commander, it shows me similar error saying cannot connect to the device.
Please give some solution for this issue.
On a completely different note,
4. I am interested in knowing how did you select the value for capacitor C15 = 100pF on the CC1350 LP. This capacitor serves as kind of a switch between on board antenna and the JSC connector for external antenna.