Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hi everybody ,
please due to project setting ( started quite long ago ) I am on CCS 5.3 , and I must stay on this one .
now when I generate binary file ( needed to later load in bootloader ) in CCS the file genarated is wrong , since first 4 byte are 0XFF .
now same project the .out file is working ( i can debig /program etc ) , and if I convert this file to HEX and then to binary it works perfectly
please what shoudl I check /change to have it working ?
here is the linking command :
-v28 -ml -mt --cla_support=cla0 --float_support=fpu32 --vcu_support=vcu0 -O2 -g --define=DEBUG --define=ENABLE_TRACE=1 --diag_warning=225 --display_error_number --asm_listing --obj_directory="C:/Users/ITENPIE/Desktop/Software/TI/CC_5/28069/EVCI_SW/obj/output/ti-debug/dev_Resonant" -z --stack_size=0x300 -m"C:/Users/ITENPIE/Desktop/Software/TI/CC_5/28069/EVCI_SW/obj/output/ti-debug/dev_Resonant/dev_Resonant.map" --warn_sections -i"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/lib" -i"C:/TI/controlSUITE/libs/math/FPUfastRTS/V100/lib" -i"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/include" --reread_libs --priority --display_error_number --xml_link_info="C:/Users/ITENPIE/Desktop/Software/TI/CC_5/28069/EVCI_SW/obj/output/ti-debug/dev_Resonant/dev_Resonant_linkInfo.xml" --absolute_exe --entry_point=code_start --rom_model
thank you
regards
carlo