This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C123GH6PM: gmake error

Part Number: TM4C123GH6PM

Tool/software: Code Composer Studio

Hello, 

I have wrote a simple example for internal CPU temperature measurement using TivaWare and CCS 7.3

Now i have CCS 8.0 ...

after importing the same project and building i have warning says that the project was made with a older version of compiler the following errors: 

gmake: *** [main.obj] Error 1

gmake: Target 'all' not remade because of errors.

the fix the warning issue by upgrading the compiler version but the errors still. 

any help? 

Thanks, 

Sarea

  • Hi Sarea,
    Can you post your full build output? I'm looking for all the messages that appeared in the build console.

    Thanks
    ki
  • Hello,
    I haven’t heard back from you, I’m assuming you were able to resolve your issue. If not, please post a reply with an update below (or create a new thread).

    thanks,
    ki