This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F2808: CCS v6.2.0.00048 history of updates

Part Number: TMS320F2808


Tool/software: Code Composer Studio

Hello all,

please can anybody tell me where I can find in CCS a summary of updates which have been done?

I have been using CCS v6.2.0.00048. I didn't use it for several months. Now as soon as I need to use

it I wasn't able to compile the source code which I was able to compile previously. So I had an idea that

the reason of my problems could be in some updates which have been done.

Thank you in advance.

  • Hello,
    You should be able to find the update history through the installation logs:
    processors.wiki.ti.com/.../Troubleshooting_CCSv6

    However, it is doubtful that the updates are the root cause of your build errors (assuming you are still using the same compiler version). What are the exact build errors you see?

    Thanks
    ki
  • Hello Ki,

    thank you very much for your reaction. I have following errors during

    linking:

    undefined first referenced
    symbol in file
    --------- ----------------
    _ausschalten_FZGEN ./XYZ.obj
    _ausschalten_MW       ./XYZ.obj
    _fzgen_berechnen       ./XYZ.obj
    _pruefe_ein_aus          ./XYZ.obj
    _set_max_power         ./XYZ.obj
    _status_led                  ./XYZ.obj

    error #10234-D: unresolved symbols remain
    error #10010: errors encountered during linking; "XYZ.out" not built
    gmake: *** [XYZ.out] Error 1
    gmake: Target 'all' not remade because of errors

    I have changed some unsigned ints literal values. I haven't done any

    other changes. Then I have tried to compile the original source code

    without any changes and the result was exactly same.

  • This error is a common linker error. The details are in the link below:
    software-dl.ti.com/.../sdto_ccs_build-errors.html

    The key thing to check is to make sure the library that defines those symbols are properly being referenced by the project (usually in the linker settings). Check the library search path and library list.

    If those symbols should be coming from a source file that is part of your project, make sure those source files are still added to the project.

    Thanks
    ki
  • Hello Ki,

    the missing symbols regards source files that are part of my project. So I have verified that the source files are still added to the project. I have observed three strange things:

    a) the above mentioned error occurs irregularly (sometimes the compilation is successful even with clean at the beginning)

    b) the missing symbols aren't still the same, it depends on the compilation

    c) whenever I ignore the error message and try to rebuild without cleaning the compilation is successful but the binary produced

        has different content for each build.

  • This is very odd behavior and something that I will need a reproducible test case to investigate further. Would it be possible to provide one? Contact me via private message if you do not wish to share publicly.

    Thanks
    ki
  • Hello Ki,
    I have just sent you my CCS project in the attachment of private message.
  • Issue was resolved off-line. The issue was determined to be caused by some security software running on the computer.

    ki