Part Number: TMS320F2806
Tool/software: TI C/C++ Compiler
This is a C2000 project. I have specified both a stack and heap section in the C2000 Linker/Basic Options. I see on the Linker command line, --heap_size=0x200 --stack_size=0x200, which is accurate. However in the .map file I do not see any reference to a Heap (ie .esysmem).
If I add a call to malloc() in my code a .esysmem suddenly does appear in the .map file, with a size of 0x200 as requested.
I'm not using malloc() but I am using sprintf() so I do want a Heap.
Why is a .esysmem not showing up in the .map file in this case?
Maybe it's part of the .ebss section?
Seems odd that it doesn't generate a .esysmem section in this case...
Thank you.