This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6713B: gmake: *** [main.obj] Error 1

Part Number: TMS320C6713B


Tool/software: Code Composer Studio

I am trying to run the simple audio loopback code available in ti site on tms320c6713.However I am getting the following errors.I have attached the dsk6713bsl.lib file and the source file.Please help.

"C:/C6713_lib/headerfiles/csl_chiphal.h", line 267: fatal error #35: #error NO CHIP DEFINED (use -dCHIP_XXXX where XXXX is chip number, i.e. 6201)
1 fatal error detected in the compilation of "../main.c".
Compilation terminated.
gmake: *** [main.obj] Error 1
gmake: Target 'all' not remade because of errors.

**** Build Finished ****

  • Hello,

    Salini Mahapatra said:
    "C:/C6713_lib/headerfiles/csl_chiphal.h", line 267: fatal error #35: #error NO CHIP DEFINED (use -dCHIP_XXXX where XXXX is chip number, i.e. 6201)

    It is as the error says. You need to define a CHIP as specified. Try defining "CHIP_6713" in your project compiler build option.

    Thanks

    ki