This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C1294NCPDT: gmake: *** [main.obj] Error 1

Part Number: TM4C1294NCPDT


Tool/software: Code Composer Studio

I am new to CCS, I am using TM4C1294 for SPI communication SSI0 as Master and SSI2 as slave, and I am receiving this error.

Given below is the code and I am getting following errors:

Description                                Resource              Type
gmake: *** [main.obj] Error 1    TMSPI             C/C++ Problem
Description                                                                        Resource                                        Type
gmake: *** [tm4c1294ncpdt_startup_ccs.obj] Error 1    TMSPI                                     C/C++ Problem


Description                                                                   Resource               Type
gmake: Target 'all' not remade because of errors.    TMSPI             C/C++ Problem

#include <stdbool.h>
#include <stdint.h>
#include <string.h>
#include "inc/hw_memmap.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/ssi.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"



#define NUM_SSI_DATA 15

/*SSI init function*/
//*****************************************************************************
//
// This function sets up UART0 to be used for a console to display information
// as the example is running.
//
//*****************************************************************************
void
InitConsole(void)
{
    //
    // Enable GPIO port A which is used for UART0 pins.
    // TODO: change this to whichever GPIO port you are using.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    //
    // Configure the pin muxing for UART0 functions on port A0 and A1.
    // This step is not necessary if your part does not support pin muxing.
    // TODO: change this to select the port/pin you are using.
    //
    GPIOPinConfigure(GPIO_PA0_U0RX);
    GPIOPinConfigure(GPIO_PA1_U0TX);

    //
    // Enable UART0 so that we can configure the clock.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);

    //
    // Use the internal 16MHz oscillator as the UART clock source.
    //
    UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);

    //
    // Select the alternate (UART) function for these pins.
    // TODO: change this to select the port/pin you are using.
    //
    GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

    //
    // Initialize the UART for console I/O.
    //
    UARTStdioConfig(0, 115200, 16000000);
}

void ssi_init(void)
{
    uint32_t ui32SysClkFreq;
    uint32_t temp;

    ui32SysClkFreq = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    GPIOPinConfigure(GPIO_PA2_SSI0CLK);
    GPIOPinConfigure(GPIO_PA3_SSI0FSS);
    GPIOPinConfigure(GPIO_PA4_SSI0XDAT0);
    GPIOPinConfigure(GPIO_PA5_SSI0XDAT1);
    GPIOPinTypeSSI(GPIO_PORTA_BASE,GPIO_PIN_5|GPIO_PIN_4|GPIO_PIN_3|GPIO_PIN_2);

    SSIConfigSetExpClk(SSI0_BASE, ui32SysClkFreq, SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 10000, 8);
    SSIEnable(SSI0_BASE);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);  //Enable ssi2
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD); //Enable PORT B GPIO to be used with ssi2 data and frame signals

    GPIOPinConfigure(GPIO_PD3_SSI2CLK);
    GPIOPinConfigure(GPIO_PD2_SSI2FSS);
    GPIOPinConfigure(GPIO_PD1_SSI2XDAT0);
    GPIOPinConfigure(GPIO_PD0_SSI2XDAT1);
    GPIOPinTypeSSI(GPIO_PORTD_BASE,GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);

    SSIConfigSetExpClk(SSI2_BASE, ui32SysClkFreq, SSI_FRF_MOTO_MODE_0, SSI_MODE_SLAVE, 10000, 8);
    SSIEnable(SSI2_BASE);
}


/*function to read the data from ssi0 in ssi2 and write it back to ssi0 and compare both*/
void main(void)
{
    uint32_t ui32Index;
    uint32_t ui32Data;
    char spi_data_received_back[NUM_SSI_DATA];
    uint32_t spi_received_char;
    const char spi_test_command[NUM_SSI_DATA] = {"This is a test\0"};
    bool pass_or_fail;

    InitConsole();
    ssi_init();

    memset(spi_data_received_back, '\0', NUM_SSI_DATA);
    for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
    {
        ui32Data = spi_test_command[ui32Index];
        SSIDataPut(SSI0_BASE, ui32Data);
        // SSIDataGet waits until a character is received
        SSIDataGet(SSI0_BASE, &spi_received_char); // Dummy read to empty master rx buffer
        SSIDataGet(SSI2_BASE, &spi_received_char); // Get data from slave rx buffer
        SSIDataPut(SSI2_BASE, spi_received_char);  // send back to master
        spi_data_received_back[ui32Index] = (char)spi_received_char;
    }
    if(strcmp(spi_test_command, spi_data_received_back) == 0)
    {
        pass_or_fail = 1;
        UARTprintf("\n\rPASSED\n\r");
    }
    else
    {
        pass_or_fail = 0;
        UARTprintf("\n\rFAILED\n\r");
    }

    return;
}

  • Snehal Deshmukh said:
    Description                                Resource              Type
    gmake: *** [main.obj] Error 1    TMSPI             C/C++ Problem
    Description                                                                        Resource                                        Type
    gmake: *** [tm4c1294ncpdt_startup_ccs.obj] Error 1    TMSPI                                     C/C++ Problem

    This summary message just says that there was an error but doesn't give further indication as to the source of the error.
    Please take a look at the CCS build console which should provide more detailed error messages, typically even the line of error if it is a compiler error. Also this page describes some of the common CCS build errors and might point in the right direction to identify the source of error:
    http://software-dl.ti.com/ccs/esd/documents/sdto_ccs_build-errors.html

    If you are still unable to resolve it using the above references, then please post the complete build log.

  • I still cannot find a solution for this errors.
  • As Aarti requested in her previous post, please provide ALL the build messages in the build console:
    software-dl.ti.com/.../sdto_ccs_build-errors.html

    Thanks
    ki
  • Console Window

    undefined       first referenced
      symbol             in file     
     ---------       ----------------
     UARTStdioConfig ./main.obj      
     UARTprintf      ./main.obj      
     
    error #10234-D: unresolved symbols remain
    error #10010: errors encountered during linking; "SLAVETM4.out" not built
     
    >> Compilation failure
    makefile:143: recipe for target 'SLAVETM4.out' failed
    makefile:139: recipe for target 'all' failed
    gmake[1]: *** [SLAVETM4.out] Error 1
    gmake: *** [all] Error 2

    **** Build Finished ****

  • Snehal Deshmukh said:
    undefined       first referenced
      symbol             in file     
     ---------       ----------------
     UARTStdioConfig ./main.obj      
     UARTprintf      ./main.obj      
     
    error #10234-D: unresolved symbols remain

    This is a key error.

    Why are you getting this error? Please see:

    http://software-dl.ti.com/ccs/esd/documents/sdto_ccs_build-errors.html#linker-diagnostics

    Hint: Where UARTStdioConfig and UARTprintf defined? Make sure you have that source/library as part of your project.

    Thanks

    ki

  • Hello,
    I do not know am example your project is derived from.
    You need to include something like uartstdio.c into your project, probably.
    Just import the timers example and check how UARTStdioConfig() and UARTprintf() are defined and implemented.