This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
I have been recently upgraded to a windows 10 machine (previously W7) and am attempting to recreate our environment which is running CCS V6.1.2.
I have researched many of the other issues shared on this forum and have already attempted the following:
- Utilized offline installer (disabling anti-virus is a no-go)
- Removed the 2005, 2010 and 2012 MSVC redistributables and re-installed (rebooted afterwards)
- Tried offline installer for CCS V6.1.3.00034
As far I as I can tell, none of this seems to help and I see the same error. Issue appearsto be while installing the emulation package? I attempted to install the latest emulation package separately (ti_emupack_setup_8.0.27.9_win_32.exe) and that seemed to install without any issues . . .
I have been deleting the install directory in between attempts, logs are attached. Any help is appreciated.
Hi Edward,
The logs you've posted are from the 6.1.2 install. They show that you're failing to install a third party emulator from Spectrum digital. If you don't need it, could you try installing without the SD component? Let me know if that works for you.
Btw, official support for Windows 10 started at 6.1.3.
Danish
Hi Danish,
Thanks for the reply. I did see a note that windows 10 support started at 6.1.3, but that doesn't seem to have done the trick. I re-attempted the installs (for both 6.1.3 and 6.1.2) without the SD component, and the installation seemed to progress a bit more but still failed.
I will be utilizing SD probes XDS200 and XDS510LC, so would like to have that support in there.
Logs for all 3 attempts are attached.
install_logs_613.7zinstall_logs_612_noSD.7zinstall_logs_613_noSD.7z
HI Edward,
Was 7.4.0 failing on SD again? Could you install without SD for now? We can add it in later. CCS is now up to version 8.1.0, btw.
Danish