This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CODECOMPOSER: V6.1.2 Windows 10 install issue

Part Number: CODECOMPOSER

Tool/software: Code Composer Studio

Hello,

I have been recently upgraded to a windows 10 machine (previously W7) and am attempting to recreate our environment which is running CCS V6.1.2. 

I have researched many of the other issues shared on this forum and have already attempted the following:

- Utilized offline installer (disabling anti-virus is a no-go)

- Removed the 2005, 2010 and 2012 MSVC redistributables and re-installed (rebooted afterwards)

- Tried offline installer for CCS V6.1.3.00034

As far I as I can tell, none of this seems to help and I see the same error. Issue appearsto be while installing the emulation package? I attempted to install the latest emulation package separately (ti_emupack_setup_8.0.27.9_win_32.exe) and that seemed to install without any issues  . . . 

I have been deleting the install directory in between attempts, logs are attached. Any help is appreciated.

6237.install_logs.7z