Tool/software: Code Composer Studio
I'm having the same problem. I have a Windows 10 and require a separate, local machine administrator account to install programs. I've installed the TICloudAgent twice; once into the administrator account (c:\Users\admin_account\TICloudAgent) as well as my network user account (c:\Users\network_account). I can get it to work if I run Chrome as admin_account, but not as network_account. I can manually run the ticloudagent.bat file in a command window and it responds with {"port":62808, "version":"4.6"} which makes me think that it can run, but it's not looking in the right place. BTW, after installation, the files were owned by the admin_account user and I switched them to the network_account user, but still, no dice.
Thanks