Other Parts Discussed in Thread: CODECOMPOSER, AM1806
I see the the LogicPD eXperimantal Board for the 1806 comes with CodeComposer.
Do I get a full license with that? Can I use it to develop/debug Linux applications?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CODECOMPOSER, AM1806
I see the the LogicPD eXperimantal Board for the 1806 comes with CodeComposer.
Do I get a full license with that? Can I use it to develop/debug Linux applications?
Josh Conn said:Do I get a full license with that?
Most likely you get the free bundled license.
Josh Conn said:Can I use it to develop/debug Linux applications?
There is some limited Linux debug support on the ARM9 with CCSv4, more useful for low level driver development than application debug. See this page for more details:
http://processors.wiki.ti.com/index.php/Linux_Aware_Debug
CCSv5 may be what you want for Linux application level debug. See this thread for more infromation:
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/61266.aspx
Thanks
ki
Josh,
I don't see an AM1806 experimenter board at LogicPD's webpage, therefore you should contact them for details on this particular model.
The development boards usually come with a copy of CCSv4 and either an embedded or a XDS100v2 emulator that allows using CCSv4 Free Limited License. For details on the Free Llimited License check:
http://processors.wiki.ti.com/index.php/Licensing_-_CCSv4#Free_Licenses
The Free Limited License allows Linux debugging on CCSv4. For details please check:
http://processors.wiki.ti.com/index.php/Linux_Aware_Debug
Still in beta, CCSv5 will also have additonal GDB support that allows additional flexibility to perform Linux debugging. Check:
http://processors.wiki.ti.com/index.php/Category:Code_Composer_Studio_v5
Hope this helps,
Rafael