This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM437X: CCS Debugger Target Connection

Part Number: PROCESSOR-SDK-AM437X
Other Parts Discussed in Thread: AM4378

Tool/software: Linux

I have CCS 7.4.0 on my window PC, and AM437x GP EVM connect the micro USB to PC USB. 

I setup the .ccxml file as the following:

Texas Instruments XDS110 USB Debug Probe

AM4378

I tried to Test Connection and got the following messages:

[Start: Texas Instruments XDS110 USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\10057284\AppData\Local\TEXASI~1\
CCS\ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Nov 6 2017'.
The library build time was '10:36:36'.
The library package version is '7.0.100.0'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.

The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.

[End: Texas Instruments XDS110 USB Debug Probe_0]

What would be my problem?

Thanks.

  • Zhiwei Wang said:

    I have CCS 7.4.0 on my window PC, and AM437x GP EVM connect the micro USB to PC USB

    I setup the .ccxml file as the following:

    Texas Instruments XDS110 USB Debug Probe

    The EVM has an onboard XDS100v2, not an XDS110. If you are connecting the EVM to your PC via USB cable, then you need to specify the XDS100v2 USB Debug Probe instead.

    Thanks

    ki