Tool/software: Code Composer Studio
I have recently procured TI's - piccolo -F28027 lauchpad.
It refuses to connect.
I am trying to run the basic LED blink program but it shoots this error:
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 8.0.27.9)
I have done all tasks relating to debugging this issue mentioned in various other threads:
1. Reinstalled CCS with selection of all types of Emulation and USD debug probes.
2.Reinstalled XDS100 device drivers.
i m not understanding the issue, the device is showing up
from command prompt it is clear that it the device is detected, thereby the drivers are also installed properly.
UART connection is working with default temp sensor code as shown.
Please rectify this issue
error is shown,
please reply as soon as possible.