This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100v1 usb emulator problem Error (-151)



Hello,

We have a problem about TMDSHVMTRPFCKIT. Week ago we installed ccs and run sample codes. Then, something happend and we got usb problem. Computer couldnt recognize drivers. I just re-install drivers(I believe, I did it right). I realize M3- LD1 doesn't turn on. When I try to debug, I got Error -151.

The value is '-151' (0xffffff69). The title is 'SC_ERR_FTDI_OPEN'.

The explanation is: One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located.


I'm new at this. Please help me.

I'm using Win7-64bit and CCS 5.3.0