This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Error: target is not connected

Tool/software: Code Composer Studio

hey guys,

im currently trying to run a lab file on my pmsm which should identify motor parameters. so i build the file in ccs and then debug it with the real-time mode. according to the lab i change two flags (in the expressions-window) and the motor starts spinning as it should. but after some time it stops and gives me the following error in my expressions-window:

Could not read 0x0BBC3@Program: target is not connected (Decimal)   

any ideas how i can fix this?

thanks in advance!