Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO: CCSv6 - Installing com.ti.ccstudio.debugserver.linux problem on Ubuntu 16.04

Part Number: CCSTUDIO

Tool/software: Code Composer Studio

Hi,

I'm having problems installing the Code Composer Studio V6.1.2 into Ubuntu v16.04. The installation stops when it tries to install the com.ti.ccstudio.debugserver.linux.

--------------------------------------------------------------------------------------------------------------
Installing... com.ti.ccstudio.debugserver.linux...
Registering com.ti.ccstudio.debuserver.linux...
Unable to download ti_dspack_ibsetup_6.1.0.1449.bin. Trying again.
--------------------------------------------------------------------------------------------------------------

It follow attached the install.log file
/ccs_setup_6.1.2.00015_install.log

I tried to install the online and the offline versions but I have the same problem.

  • Hello Milan,
    Any reason why you are trying to use 6.1.2? It is quite an old version I would like to suggest installing something more recent, if you can. Is your Ubuntu distro a 32-bit one?

    Thanks
    ki
  • Hello Ki,

    Yes, the reason is that I have some code as a motor controller adjusted for this specific (and older) version(s) of CCS and I would like to use the advantage of this code which is couple of years old. The main reason is the code uses patched 64bit Ubuntu 16.04 kernel making it Real-Time Linux. But, nevertheless I tried with both 32bit and 64bit generic distros (without patching kernel). To sum up, the same error occurs on generic 32bit, generic 64bit and on preempt-real time linux 64bit kernel patched Ubuntu 16.04 kernel.

    Thank you,
    Milan