This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I have an MSP430 project with a large number (64) of build targets, each building a slightly different variation of a product. The difference between each come down to part number, and a few configuration switches.
Recently I've run into a problem where switching the compiler version on ONE target causes the .cproject file to be re-written in such a way as to default almost all the individual settings for all of the build targets.
This means the linker command file is defaulted, the include paths are defaulted, the pre-defined symbols are defaulted. Additionally the linker paths and included libraries get defaulted as well. The MPU support gets turned on as well, and probably a few other changes I haven't caught yet.
Needless to say, with 64 targets, this is a humongous pain. I've tried with CCS V8.1 8.2 and 7.3, and the same thing happens with all of them. I suspect that something has become corrupted in my .cproject file, and that's triggering the issue, but I'm not sure what it could be.
Are there any logs I could look at or other troubleshooting techniques I could use to narrow down the cause of this?
Regards,
Josh - AFD Engineering.
Josh,
Could you share your original .cproject file (prior to switching the compiler version) and the one it gets updated to after the change? You can zip them up and attach them here. Or if you prefer to share them privately, you can send me a private message (by hovering over my forum ID).
I'm not sure if that alone will be sufficient to root cause the issue but let us start there.