Other Parts Discussed in Thread: CC2640R2F
Tool/software: Code Composer Studio
Hi
I am using simplelink cc2640r2d launchpad for BLE testing and sample program development.
I had downloaded CCS offline for the same.
Then i had gone through to development guide for CC26XX wireless modules. Link of the same is given below. (Link1)
Then according to document as far as i understand i need ble_sdk_2_02_02 something .exe file for BLE. I downloaded it and execute in my windows.
Then while debugging the project for my LAUNCHPAD while it is connected with system with USB cable, I had seen the error that this module you had selected is not compatible for CC2640R2F.
I had followed these steps.
Create a workspace.
1. Ensure that the CCS workspace path does not contain a whitespace.
2. Open the CCS IDE from the Start Menu.
3. Select Project→ Import CCS Project.
4. Select $BLE_INSTALL$\examples\cc2650em\simple_peripheral\ccs. NOTE: This is the CCS directory for the simple_peripheral project. CCS discovers two projects (the application project and the stack project).
5. Click the box next to an application project (depending on your development platform) and the stack project to select them.
6. Select Copy projects into workspace.
Then after debugging the result is error. Then i had tried all examples the result is same for all.
Then i had downloaded the referred SMARTRF FLASH PROGRAMMER 2 as adviced in that developer guide document to burn already present hex files in LAUNCHPAD.
Then it shows FAIL. with error (4).
Then LAUNCHPAD document on ti site i had seen that we need simple link sdk for this launchpad. That file name is "simplelink_cc2640r2_sdk_2_30_00_28".
I download this file and try to open some example in CCS. Then i see that there is no project file in any example there are only ".C"0 files in there.
When i see online version of "simplelink_cc2640r2_sdk_2_30_00_28" in "dev.ti.com/tirex" i had seen all the project files are there in those example.
Is there any possible way to download those project file for offline use.??