This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi there,
When I debugging simple_broadcaster example of BLE5 stack from sdk 2.30.00.28, objectviewer can not show anything on task details.
it says "Error: java.lang.Exception: Target memory read failed at address: 0x20001b10, length: 76 This read is at an INVALID address according to the application's section map. The application is likely either uninitialized or corrupt."
I am using ccs8.3 the latest.
update : seems there is same problem on other example of BLE5 stack, like simple_peripheral:
"Error: java.lang.Exception: Target memory read failed at address: 0x20001ecc, length: 76 This read is at an INVALID address according to the application's section map. The application is likely either uninitialized or corrupt."
Thank you Todd,
1. Does ROV classic have the same behavior?
yes, the same.
2. Does either ROV tools work properly while in main()?
I am not so sure about what other ROV tools you want me to check?
3. Can you view that memory location in a Memory Browser?
like this,
4. How do you load the target? Via CCS or some other mechanism?
with CCS debug directly, not other mechanism.
Best regards and happy new year!
Hi Todd,
1. Regarding #2, when you are at the start of main(), open ROV. Do you get the "Error: java.lang.Exception: Target memory read failed at blah blah." error then?
At the start of main(), ROV(explore tasks) is working right.
After ICall_createRemoteTasks(), ROV(explore tasks) says "Error: java.lang.Exception: ..."
B.R.