Part Number: MSP-FET430UIF
Other Parts Discussed in Thread: MSP-FET
Tool/software: Code Composer Studio
Using MSP-FET430UIF emulator and target MSP4304538A evaluation board with
Version: 8.0.0.00016
2) IAR Embedded Workbench for MSP430 7.12.1 (7.12.1.987)
and get errors when try to download and debug
in IAR (first I been ask to Update the firmware now the version is 3.11.00.001 and in the device manager I see (COM17 MSP-FET430UIF -CDC)) now I get message
Fatal error: Failed to re-initialize
session aborted!
in CCS I get error message
Error connecting to the target:
Unknown device
(when test identify it find some FET device)
in FET - Por 430 error message
=====================================
JTAG communication initialization.... failed
Verifying Security Fuse .................... failed
--------------- FAILED !!! -----------------
can some one rely help to solve the problem (the connection to external emulator become hard to establish)
if using older version of IDE is needed please write the number
Kind Regards
David
david-p51@013.net.il