This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1443BOOST: CCS build error: #1965: cannot open source file "mmw_lvds_stream.h"

Part Number: IWR1443BOOST


Tool/software: Code Composer Studio

When I tried to build SDK demo, I met  this problem.

Compilation failure
subdir_rules.mk:9: recipe for target 'sensor_mgmt.obj' failed
"..\mmw.h", line 60: fatal error #1965: cannot open source file "mmw_lvds_stream.h"
1 catastrophic error detected in the compilation of "../sensor_mgmt.c".
Compilation terminated.
gmake[1]: *** [sensor_mgmt.obj] Error 1
gmake[1]: Target 'main-build' not remade because of errors.
gmake: *** [all] Error 2
makefile:160: recipe for target 'all' failed

Also, I have another question about CRC.pm.

I use option eclipse marketplace to download EPIC. But I can't find the install directory and I can't find CRC.pm.

How do I know that I meet all the conditions especially Perl and CRC.pm ?

  • Hello,

    Which SDK version are you using?

    user5948132 said:

    Also, I have another question about CRC.pm.

    I use option eclipse marketplace to download EPIC. But I can't find the install directory and I can't find CRC.pm.

    How do I know that I meet all the conditions especially Perl and CRC.pm ?

    I'm not sure I understand your question. You can indeed download and install EPIC from the Eclipse Marketplace. But I don't understand your question about the installation directory. It will install EPIC as a plugin to CCS. Note that does NOT install Perl itself. As for CRC.pm file, this is a question best asked to the SDK experts in the device forum.

    Thanks

    ki

  • OK. Thanks.
    And the SDK version I used is 1.2.
  • Try updating the SDK version and the toolkit version. I used SDK version 2.1.
  • Hello,
    I haven’t heard back from you, hence this issue is being closed. If you wish to continue the discussion, please post a reply with an update below (or create a new thread).

    Thanks,
    ki