Part Number: C2000-CGT
Other Parts Discussed in Thread: CCSTUDIO
Tool/software: TI C/C++ Compiler
Hi,
Is there a way to build all the build configurations available in a CCS project from command line?
I saw one E2E query on the same topic and the suggestion was to have a batch file which calls the CLI command to build individual build configuration. Is there a way to get the build configuration names as well from CLI?
The problem I have is I need to build multiple projects. Currently I am using a loop to iterate through all the projects and build them. But there are projects with multiple build configurations. Is there a way to get those other than hard coding them in the script
Thanks!
Veena