This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
I am trying to do a headless build on a project that has multiple configurations.
I am using command line prompt on windows 7 (64 bit) with Code Composer Studio version 6.2.
When doing a project build with, say, CONFIG-A (set using "-css.configuration CONFIG-A"), the headless build is successful and generates the required files. However, when I try to build with configuration CONFIG-B, it still executes the build with configuration CONFIG-A. Both the build commands are given after importing the project.
Am I missing something? Is this a CCS6.2 issue?
hello,
Raj K1 said:Is this a CCS6.2 issue?
no, it should work in CCSv6.2
Raj K1 said:Am I missing something?
I think the issue is a typo in the command:
Raj K1 said:(set using "-css.configuration CONFIG-A")
note the typo above. It should be:
-ccs.configuration
Because of the typo, the parameter is likely being ignored. Hence it will always default to the last configuration used (CONFIG-A)
Thanks
ki