Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi,
I'm in the process of setting up a new project and am following the F28004x Firmware Development Package User's Guide. Section 2.3 states that Driverlib and Bitfield libs are "...implemented to be compatible together within the same user application."
I followed the instructions for "Adding Driverlib Support" and "Adding Bitfield Support" to my project. (Which was previously compiling successfully with only driverlib support)
Afterwards, when I tried to build the project I get the following errors:
subdir_rules.mk:23: recipe for target 'main.obj' failed
"C:\ti\C2000Ware_1_00_06_00_Software\device_support\f28004x\headers\include\f28004x_lin.h", line 236: error #41: expected an identifier
"C:\ti\C2000Ware_1_00_06_00_Software\device_support\f28004x\headers\include\f28004x_lin.h", line 236: error #80: expected a type specifier
"C:\ti\C2000Ware_1_00_06_00_Software\device_support\f28004x\headers\include\f28004x_lin.h", line 236: error #170: a function type is not allowed here
Line 236 in ...\f28004x_lin.h is defining a bitfield as the following:
bp_16 IDLE:1; // 2 SCI receiver in idle state (SCI compatible mode)
The problem appears to be that IDLE is also being defined in ...\driverlib\f28004x\driverlib\cpu.h as:
#ifndef IDLE
#define IDLE __asm(" IDLE")
#endif
Any suggestions?
Thanks,
Isaac