This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have a .lib file that was created from C674x PSP. I'm trying to figure out how the build was done so it can be recreated. Is there compiler/linker information embedded in the .lib file that can be extracted? I'd like to know what version of the compiler was used and what compile options were used.
As it stands, we can include this library in our application, but if I rebuild the library and then re-link our application, it won't build because the library takes up too much memory - even when I set the library build to the most aggressive settings for reducing memory size. The weird thing is, the default library size that works (e.g. the currently used .lib file) is 163 kB. I can rebuild it such that the size goes down to 132 kB but when I link this in with our application, it won't build because it runs out of memory. My conclusion is that the linking in the rebuilt library is now taking more memory than the default build.
So, ideally I'd like to somehow find out what compile settings were used on our default .lib file. Or just figure out how to re-build the .lib file so that it will take up the same or less memory versus our default .lib build.
Also, is there a compile/link option we can set for archive builds that will log all the settings used to build the library?
thanks,
Mike
You can extract the version of the assembler used to build the library member object files by running ofd6x over the library archive. The version of the assembler will correspond to the version of the compiler used to build the library. Most command-line options are not recorded explicitly in the object file.
What is it that is running out of memory? Is your desktop machine running out of memory, or is the program too big for the target you are compiling for?
The size of the library archive is not a good indicator of how big its target footprint is; it contains meta-information like debugging information and uninitialized sections which can be much larger on the target than in the archive.
thanks for the response.
Archaeologist said:What is it that is running out of memory? Is your desktop machine running out of memory, or is the program too big for the target you are compiling for?
The linker operation fails because code can no longer be placed in IRAM whereas previoiusly it all fit in IRAM. It's not a windows crash.
Your suggestion of is ofd6x is good, except we didn't put .obj files in our source control. Just the .lib file. I'll try and build with different combinations to see what makes it build. What options should I use to reduce memory usage in the application linking in the library?
thanks,
Mike
Mike said:Your suggestion of is ofd6x is good, except we didn't put .obj files in our source control. Just the .lib file. I'll try and build with different combinations to see what makes it build. What options should I use to reduce memory usage in the application linking in the library?
A library is just an archive of object files; your object files are intact inside the archive, and ofd6x can read them.
Try using the -ms compiler option to favor optimizing for smaller code size. You should probably use optimization as well, even though some optimizations can increase code size. The idea is -ms tries to keep that under control.
See http://processors.wiki.ti.com/index.php/C6000_Compiler:_Recommended_Compiler_Options
What sort of factor increase in code footprint are you seeing? Is it right on the edge, or something like 2x?
This is all good help. I ran ofd6x on the original and re-built lib files. Both use compiler 6.1.12. I still need to rearrange things to see what the footprint differences are. But one thing that jumps out is the size of the .far sections. The re-built lib is much bigger. Why is this?
Here is cut/paste from the of6dx output:
original .lib file:
7 .const 0x00000000 0x00000000 0x10c 4 Y
8 .far 0x00000000 0x00000000 0x1b08 4 Y
9 .text:_mcaspMdUnBindDev 0x00000000 0x00000000 0x60 32 Y
rebuilt .lib file:
7 .const 0x00000000 0x00000000 0x10c 4 Y
8 .far 0x00000000 0x00000000 0x637c 8 Y
9 .text:_mcaspMdUnBindDev 0x00000000 0x00000000 0x60 32 Y
I'll try and rearrange some memory so the project builds and tell you what the footprint difference is.
thanks.
".far" is for data, so this is not a code size issue. Is there a corresponding drop in size for the ".bss" section? If yes, then it's being compiled for a different data memory model.
Whether data is placed in ".far" or ".bss" depends on the memory model. See http://processors.wiki.ti.com/index.php/C6000_Memory_models
No. bss is the same. I'll cut/paste the first lines of output of ofd6x run on each library. .far still takes up space in the memory map. IRAM contains code and data so I'm pretty sure now the reason the link can't place the re-built library in memory is that the .far section is too big for IRAM. Any other suggestions why .far is so much bigger on the re-built library? I can attach the whole ofdx6 output files if that will help.
original lib output of ofd6x:
ARCHIVE: ti.pspiom.mcasp_3_3.lib
OBJECT FILE: Mcasp.obj
Object File Information
File Name: Mcasp.obj
Format: TI-COFF Version 2
File Type: relocatable file
Time Stamp: Mon Jul 12 14:45:27 2010
Machine: TI C6x
Machine Endian: little endian
Entry Point: 0x00000000
Vendor: Texas Instruments, Inc.
Producer: Assembler
Assembler Version: 6.1.12
Number of Sections: 60
File Length: 88742
File Offset in Archive: 1008
Symbol Table File Offset: 0x00012d39
String Table File Offset: 0x00014db5
TI-COFF f_flags: 0x00000190
CPU Generation: C6740
Control Data Endian: little endian
Section Information
id name load addr run addr size align alloc
-- ---- --------- -------- ---- ----- -----
1 $build.attributes 0x00000000 0x00000000 0x21 1 N
2 .text 0x00000000 0x00000000 0x0 1 Y
3 .data 0x00000000 0x00000000 0x0 1 Y
4 .bss 0x00000000 0x00000000 0x4 4 Y
5 .debug_info 0x00000000 0x00000000 0x7a53 1 N
6 .cinit 0x00000000 0x00000000 0x3c 8 Y
7 .const 0x00000000 0x00000000 0x10c 4 Y
8 .far 0x00000000 0x00000000 0x1b08 4 Y
9 .text:_mcaspMdUnBindDev 0x00000000 0x00000000 0x60 32 Y
10 .text:_mcaspWriteChanS... 0x00000000 0x00000000 0xe0 32 Y
11 .text:_mcaspWriteUserD... 0x00000000 0x00000000 0xe0 32 Y
12 .text:_Mcasp_localGetN... 0x00000000 0x00000000 0x20 32 Y
re-built lib output of ofd6x:
ARCHIVE: ti.pspiom.mcasp_3_3.lib
OBJECT FILE: Mcasp.obj
Object File Information
File Name: Mcasp.obj
Format: TI-COFF Version 2
File Type: relocatable file
Time Stamp: Thu Dec 02 08:37:18 2010
Machine: TI C6x
Machine Endian: little endian
Entry Point: 0x00000000
Vendor: Texas Instruments, Inc.
Producer: Assembler
Assembler Version: 6.1.12
Number of Sections: 60
File Length: 90067
File Offset in Archive: 1008
Symbol Table File Offset: 0x000131c4
String Table File Offset: 0x000152e2
TI-COFF f_flags: 0x00000190
CPU Generation: C6740
Control Data Endian: little endian
Section Information
id name load addr run addr size align alloc
-- ---- --------- -------- ---- ----- -----
1 $build.attributes 0x00000000 0x00000000 0x21 1 N
2 .text 0x00000000 0x00000000 0x0 1 Y
3 .data 0x00000000 0x00000000 0x0 1 Y
4 .bss 0x00000000 0x00000000 0x4 4 Y
5 .debug_info 0x00000000 0x00000000 0x7bd8 1 N
6 .cinit 0x00000000 0x00000000 0x3c 8 Y
7 .const 0x00000000 0x00000000 0x10c 4 Y
8 .far 0x00000000 0x00000000 0x637c 8 Y
9 .text:_mcaspMdUnBindDev 0x00000000 0x00000000 0x60 32 Y
10 .text:_mcaspWriteChanS... 0x00000000 0x00000000 0xe0 32 Y
11 .text:_mcaspWriteUserD... 0x00000000 0x00000000 0xe0 32 Y
12 .text:_Mcasp_localGetN... 0x00000000 0x00000000 0x20 32 Y
thanks,
Mike
Is that all of the sections for each of these two lists? If so, the total size of all data sections is a lot larger in the re-build, which typically does not happen by changing compiler options.
The most likely cause is a change in the source code, such as a buffer defined with a different length, possibly through command line defines. Could you characterize what kind of global data the source file has?
There are some sub-sections of .text, but you're point is well taken. Something in the rebuild is picking up a lot more data (e.g. variables). I need to check previous revisions to see what could have caused this. This library is the McASP PSP for C674x so it has a lot of globals. Let me spend some time trying to run this down. I'll post my results.
thanks,
Mike
I have an idea of how you can quickly find which object file(s) contribute the increase in the size of .far. The cg_xml package includes a script named sectti. That script can, among other things, output data on the sections found in library files in .csv format. A command similar to this would collect size data on .far sections ...
$ ofd6x -x --xml_indent=0 --obj_display=none,sections,header,segments name.lib \ | sectti.exe -c | fgrep '.far' Reading from stdin ... rts64plus.lib,ecvt.obj,.far,UDATA,100 rts64plus.lib,exit.obj,.far,UDATA,12 rts64plus.lib,fcvt.obj,.far,UDATA,400 rts64plus.lib,gsmvars.obj,.far,UDATA,8 rts64plus.lib,memory.obj,.far,UDATA,8 rts64plus.lib,pprof_user.obj,.far,UDATA,4 ...
Then use Excel to process that csv data in a manner similar to how code size data is processed in this Wiki article.
Thanks and regards,
-George
Thanks to both of you for the help. The problem was a #define in the source code that would compile out unneeded buffers and code. This was not getting #defined in the re-build.
All this feedback has been helpful and will be useful tools as we try and further characterize and optimize code usage.
thanks!
Mike