Part Number: CC1352P
Tool/software: Code Composer Studio
Hi,
I updated to the new SDK for CC1352 (3.10) and am using 9.0.1 as this is one of the dependencies for the new SDK.
With 9.0.1 I can no longer set breakpoints when the code is running. I must pause first
This is similar to this post here:
I have done everyhthing that you said in that post, but it still does not work.
The TI emulator i am using is 8.1.0.00012
I have also tried deleting the workspace and the debug configuration with no luck.
Attached is a debug log
With 8.3 I dont see this issue