This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
Hi
The issue is as shown in the title.
I want to ensure if it is a version bug of CCS9.0
thanks.
use external makefile in CCS9.0, "build" dont update the .obj file and .hex file through the code has changed.
6002469 said:use external makefile in CCS9.0
I assume this means that you are NOT using a CCS Project, or an Eclipse managed make project. Is this correct? An existing makefile project is being used, of which the makefile is manually maintained by you?
Thanks
ki