This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
For security - the computer has no Internet connection.
I 1st "Un-Zip" the file ccs9.0.1.00004_win64.zip and then install it on my computer.
When I start CCS - there is "nothing" in the "Resource Explorer" - Its all Empty.
So, Where do I download the "Software Packages" to install manually in CCS?
And, How do I install the "Software Packages" when working offline in CCS?
Session ID: 1559830141733_00001602
Conroy,
Even if you download and install the software packages separately Resource Explorer requires a connection to the internet to download the associated metadata to be able to display them properly. Once it has downloaded the metadata then it can operate in offline mode without a connection to the internet.
The software package that you want for MSP430FR5994 is MSP430Ware. You can download that here: http://www.ti.com/tool/MSPWARE
You can import examples from MSP430Ware using the project import wizard in CCS.
Regards,
John