This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6655: Compiler option for generating comments on the .lst and .asm files

Part Number: TMS320C6655

Tool/software: Code Composer Studio

Hi TI

I'm dealing with some very serious compiler issues and need to look at the generated code using .lst andn .asm files.

It's very hard to read the generated code. Do you know some compile option which provides the comments in the .lst andn .asm files.?

We are using the compile version 7.4.12 and working on switching to version 8.3.3. But there is some issue we need to clarify first

Some thing like this example from one of TI's reference guide:

>>>>>>>>

Example 8-7 SPLOOPW Implementation of C Coded Loop

MVK 8,A0 ;Do 8 loops
[!A0] SPLOOPW 1        ;Check loop
LDW .D1 *A1++,A2       ;Load source value
NOP 1
SUB .S1 A0,1,A0           ;Adjust loop counter
NOP 2                            ;Wait for source to load
MV .L2X A2,B2               ;Position data for write
SPKERNEL 0,0               ;End loop
|| STW .D2 B2,*B0++       ;Store value

End of Example 8-7

<<<<<<<<<<<<<<<<<

Thanks for your help

BR

Tam Tran

Vestas Wind System