Tool/software: Code Composer Studio
I am working with a custom board built around the CC1352R (Rev C. currently) part and utilizing both sub-GHz and 2.4 GHz functionality to combine our previously running custom sub-GHz protocol with BLE functionality.
I started with the DMM Simple Peripheral & WSN Node example (C:\ti\simplelink_cc13x2_sdk_2_30_00_45\examples\rtos\CC1352R1_LAUNCHXL\dmm\dmm_wsnnode_ble_sp\) and have successfully modified everything to run as desired.
In the project, the Startup/ directory contains a board.c file which includes the (original) board specific file:
#include "./cc1352r1lp/cc1352r1lp_board.c"
That file is pulled from C:\ti\simplelink_cc13x2_sdk_2_30_00_45\source\ti\ble5stack\target\, which next includes more specific files:
#include "../../boards/CC1352R1_LAUNCHXL/Board.h"
#include "../../boards/CC1352R1_LAUNCHXL/CC1352R1_LAUNCHXL.c"
#include "../../boards/CC1352R1_LAUNCHXL/CC1352R1_LAUNCHXL_fxns.c"
from C:\ti\simplelink_cc13x2_sdk_2_30_00_45\source\ti\ble5stack\. There is also a CC1352R1_LAUNCHXL.h file that is included by Board.h and CC1352R1_LAUNCHXL.c.
I can create copies of all this in the SDK, following the same path & naming conventions, for my custom board changes, but I would much rather have these files directly in the project so that other developers do not need to modify their SDK directories. I have seen other examples that do this.
To make it simple, I replaced the original board.c file with essentially the second one, but pull in the three files from the same (current) directory. I believe that this is all correctly compiling (I removed the files from the SDK directory to be certain it was not still using those), but the link stage reports a lot of "already been defined" errors. For example:
symbol "ADC_config" has already been defined null: symbol "ADC_config" has already been defined
ADC_config is defined in CC1352R1_LAUNCHXL.c:
const ADC_Config ADC_config[CC1352R1_LAUNCHXL_ADCCOUNT] = {
{&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC1352R1_LAUNCHXL_ADC0], &adcCC26xxHWAttrs[CC1352R1_LAUNCHXL_ADC0]},
{&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC1352R1_LAUNCHXL_ADC1], &adcCC26xxHWAttrs[CC1352R1_LAUNCHXL_ADC1]},
{&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC1352R1_LAUNCHXL_ADC2], &adcCC26xxHWAttrs[CC1352R1_LAUNCHXL_ADC2]},
{&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC1352R1_LAUNCHXL_ADC3], &adcCC26xxHWAttrs[CC1352R1_LAUNCHXL_ADC3]},
{&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC1352R1_LAUNCHXL_ADC4], &adcCC26xxHWAttrs[CC1352R1_LAUNCHXL_ADC4]},
{&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC1352R1_LAUNCHXL_ADC5], &adcCC26xxHWAttrs[CC1352R1_LAUNCHXL_ADC5]},
{&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC1352R1_LAUNCHXL_ADC6], &adcCC26xxHWAttrs[CC1352R1_LAUNCHXL_ADC6]},
{&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC1352R1_LAUNCHXL_ADCDCOUPL], &adcCC26xxHWAttrs[CC1352R1_LAUNCHXL_ADCDCOUPL]},
{&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC1352R1_LAUNCHXL_ADCVSS], &adcCC26xxHWAttrs[CC1352R1_LAUNCHXL_ADCVSS]},
{&ADCCC26XX_fxnTable, &adcCC26xxObjects[CC1352R1_LAUNCHXL_ADCVDDS], &adcCC26xxHWAttrs[CC1352R1_LAUNCHXL_ADCVDDS]},
};
I have cleaned the project before building as well as manually deleting everything in the FlashROM_Release directory and continue to get these errors (~90 of them).
Is there some other output file of which I am not aware to delete?
Or are the pre-built libraries in the SDK somehow causing this? (And since they are pre-built, I assume I cannot resolve the issue?)
Thanks!
.Tim