Part Number: LAUNCHXL-F28027
Tool/software: Code Composer Studio
Emulator for C2000 and CCS9
Hi,
We are currently using the XDS100v1 facilities built into the dev kits/control cards, but we are looking at obtaining something a little more……comprehensive, specifically something that can perform in circuit emulation rather than simple debug. This is for a very sensitive application.
A number of other XDS platforms have been mentioned, but would prefer some guidance. I’ve seen some options, Spectrum Digital and Blackhawk, with the original manufacturer of the same kit being one or all of those! Very confusing.
We need a suggestion that provides:
In circuit emulation capability
- Compatible with C2000 devices.
- Compatible with CCS 9, 8 and 7 (not bothered about earlier versions)
- USB/Ethernet (not PCI based) interface
- Not about to become obsolete/unsupported
Can you advice?
Also, can you clarify the difference between XDS560v2 System Trace and ADS560v2 Pro Trace? Which is better?