Other Parts Discussed in Thread: TM4C129ENCPDT
Tool/software: Code Composer Studio
I cannot edit my project's launch configuration in CCSv9.
In Project Properties, going to Run/Debug Settings, selecting the launch configuration, and clicking Edit fails silently. No error message is shown. No dialog box opens.
I'm using CCS v9.1.0 on Linux for TM4C129ENCPDT. My project has its own makefile. I am using the CCS Linaro GCC for ARM compiler. I need my launch configuration to launch the binary that is produced by my makefile. When I create the new project and set it up, the project can build successfully. However, if I go into the launch configuration and set the program name to my binary, then exit that launch configuration dialog, I cannot edit the launch configuration again because clicking that Edit button has no effect, as mentioned before.
Going to Run -> Debug Configurations has no effect either.
I tried deleting the workspace and starting over with a new one, several times.
I tried deleting the CCS project and starting over with a new one, several times.
I was able to get this working before but that CCS project became all messed up because I tried to rename it through CCS. So I have to re-create that CCS project and everything else works, except setting up the launch configuration.
I see that other people have reported issues with this and that one of TI's staff was able to reproduce with CCSv8. It seems the problem continues into CCSv9. Reference: e2e.ti.com/.../760367