This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm building a Static Library, using CCS 4.1 and want to strip/replace all symbols, except couple functions. So if somebody unarchives the library and disassembles the object, there are no function names (or junk function names, like: func001, func002, var001, var002, ...).
Is there any simpler then manual way to do this?
PS: Library consists of ~15 objects and there are no way to define everything as static.
Thanks!
You can try using 'hide' or 'strip'
ki
Thanks Ki,
I tried it, it strips/hides symbol information pretty good. But here is a question:
But, here is what I have: library that consists of o1 and o2 object , I stripped/hide all symbols from o1.obj, and all except 1 (that I want to make "public") from o2.obj. Also o2.obj have calls to o1.obj, How the linker (later when building a binary) would know where to link this call (o1.obj got completely stripped)?
It almost looks like I need a tool that will rename all symbols (except couple that I want to share) to some generic names, like func1, func2, var1, var2, etc.
Any ideas?
mmaaxx,
I'll move this to the Compiler forum, where there is more expertise on this fetaure.
Thanks
ki
Thanks Ki, here is what I end up doing (just want to share a solution if somebody would have same problem):
1. Using nm utility, created a list of symbols in all objects.
2. Manually edited it (removed some "internal" and symbols that I want to keep untouched).
3. Created a script took a file with the list of symbols and created obfuscate.h, that looks like: