Part Number: CC2640R2F
Tool/software: Code Composer Studio
Hello colleagues,
I tried to use rename (Rename Resource) in CCS and when I try to build and debug (F11) I get the error below. It works fine if I just rename the project name in the .projectspec file before I import. Should this work? Is there an easy fix?
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Texas Instruments XDS110 USB Debug Probe/Cortex_M3_0 : Target must be connected before loading program.
Code Composer Studio
Version: 9.1.0.00010
simple_peripheral from simplelink_cc2640r2_sdk_3_20_00_21
The issue was first reported here:
https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/t/833027