This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSEMU200-U: adapter needed with debugger

Part Number: TMDSEMU200-U

Tool/software: Code Composer Studio

For the application PCB, I need an adapter like this to use with the XDS200 debugger:

https://www.digikey.com/products/en?keywords=EA-ACC-040

Is this pin to pin compatible? To use this adapter, I need to use one of the adapter boards that came with the debugger.

Thanks,

Priya

  • Priya,

    The TMDSEMU200-U already comes with a set of pin adapters - check its product page and the photographs.

    http://www.ti.com/tool/TMDSEMU200-U

    The Digi-key adapter you showed is already encompassed by the ARM 10-pin and ARM 20-pin. 

    Hope this helps,

    Rafael

  • The adapters that came with the debugger were all socket type. I need pin adapter. The connector on the application PCB is not a standard JTAG connector unfortunately. 

    The TM4C EK emulator had a pin connector for standard JTAG and an adapter board used with this is available to connect to the application PCB.

    Priya