This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
For the application PCB, I need an adapter like this to use with the XDS200 debugger:
Is this pin to pin compatible? To use this adapter, I need to use one of the adapter boards that came with the debugger.
Thanks,
Priya
Priya,
The TMDSEMU200-U already comes with a set of pin adapters - check its product page and the photographs.
http://www.ti.com/tool/TMDSEMU200-U
The Digi-key adapter you showed is already encompassed by the ARM 10-pin and ARM 20-pin.
Hope this helps,
Rafael
The adapters that came with the debugger were all socket type. I need pin adapter. The connector on the application PCB is not a standard JTAG connector unfortunately.
The TM4C EK emulator had a pin connector for standard JTAG and an adapter board used with this is available to connect to the application PCB.
Priya