This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
I'm using CCS 9.0.1 platform for UCD3138A.
But I'm facing some problems.
I'm trying to build a UCD3138A source code, but following error was appearing..
kindly help resolve it thanks in advance,
Park
Description Resource Path Location Type
#10263 .ccsproject /UCD3138_LLC_HB line 21, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 25, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 26, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 27, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 32, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 33, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 34, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 35, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 36, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 42, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 55, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 56, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 57, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10263 .ccsproject /UCD3138_LLC_HB line 58, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 21, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 25, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 26, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 27, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 32, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 33, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 34, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 35, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 36, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 42, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 55, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 56, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 57, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10264 .ccsproject /UCD3138_LLC_HB line 58, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
<a href="processors.wiki.ti.com/.../10099"> program will not fit into available cyclone.cmd /UCD3138_LLC_HB line 71 C/C++ Problem
<a href="processors.wiki.ti.com/.../10099"> program will not fit into available cyclone.cmd /UCD3138_LLC_HB line 81 C/C++ Problem
<a href="processors.wiki.ti.com/.../10234"> null: unresolved symbols remain UCD3138_LLC_HB C/C++ Problem
errors encountered during linking; "UCD3138_LLC_HB_UCD3138A.out" null: errors encountered during linking; "UCD3138_LLC_HB_UCD3138A.out" UCD3138_LLC_HB C/C++ Problem
gmake: *** [UCD3138_LLC_HB_UCD3138A.out] Error 1 UCD3138_LLC_HB C/C++ Problem
gmake: Target 'all' not remade because of errors. UCD3138_LLC_HB C/C++ Problem
unresolved symbol $c_int00, first referenced in ./load_UCD3138.obj UCD3138_LLC_HB C/C++ Problem
#10190-D .ccsproject /UCD3138_LLC_HB line 100, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10190-D .ccsproject /UCD3138_LLC_HB line 101, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10190-D .ccsproject /UCD3138_LLC_HB line 102, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10190-D .ccsproject /UCD3138_LLC_HB line 103, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10190-D .ccsproject /UCD3138_LLC_HB line 98, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10190-D .ccsproject /UCD3138_LLC_HB line 99, external location: C:\Users\PSJ\Desktop\PMP40552_Code_06262019\Device\UCD3138A\Linker\cyclone_A.cmd C/C++ Problem
#10366-D null: automatic library build: using library UCD3138_LLC_HB C/C++ Problem
#179-D function "cc_handler" was declared but never referenced interrupts.c /UCD3138_LLC_HB line 127 C/C++ Problem
This project is currently in 'manual' Parser Preprocessing mode - no dependency graph is automatically generated. This mode should only be temporarily used to generate various pre-processor listing files. Please switch the Parser Preprocessing mode back to 'automatic' for you regular builds. UCD3138_LLC_HB properties Problem
Hi,
At first glance it seems that you have either a problem with a duplicate linker cmd file or a faulty one. Despite using a different device, the thread below has a very similar scenario as yours, with similar sequence of errors.
https://e2e.ti.com/support/tools/ccs/f/81/p/708305/2610716#2610716
Can you see if the suggestions there can help you?
Regards,
Rafael