Part Number: CCSTUDIO
Tool/software: Code Composer Studio
Hi,
I want to build my CCS MSP430 project in a docker container running Ubuntu 18.04.
I think I managed to install CCS 9.1.0 using the following command line:
./ccs_setup_linux64_9.1.0.00010.bin --mode unattended --prefix /ti --response-file /home/CCS9.1.0.00010_linux-x64/response.txt
with the attached response file:
CreateDesktopShortcut: No CreateQuickLaunchShortcut: No InstallDir: /ti InstallMode: Standard LaunchApplication: No edition_selection: Custom feature_selections: IDE_MSP430 MSP430_BUILD_DEBUG MSP430_GCC_SUPPORT EMU_MSP430 JRE JRE32 P2APP ECLIPSE ECLIPSECORE P2TOOLS GMF IDE_MAIN IDE_WORKFLOW DVT_COMMON DVT_UIA DVT_VIA_CCS TIREX XULRUNNER INSTALLER IDE_CHROME IDE_TOOLS_COMMON IDE_GC TARGET_CONTENT_CORE TARGET_CONTENT_CORE_LEGACY NODEJS USERGUIDE DS DS_FLASH CLOUDAGENT SYSCONFIG MSVC80 MSVC2012 MSVC2015 MSP430_CGT_HELP CGT_DEFAULTLIBS_MSP430 DMED GCC_MSP430_COMPILER DVT_ENERGYTRACE product_selections: PF_MSP430
Then, when I try to build my project using this command line:
eclipse -noSplash -data <workspace> -application com.ti.ccstudio.apps.projectBuild -ccs.project <project>
I get the following error:
!MESSAGE Application error
!STACK 1
java.lang.RuntimeException: Application "com.ti.ccstudio.apps.projectBuild" could not be found in the registry. The applications available are: org.eclipse.ant.core.antRunner, org.eclipse.cdt.codan.core.application, org.eclipse.cdt.core.GeneratePDOM, org.eclipse.cdt.core.CodeFormatter, org.eclipse.cdt.managedbuilder.core.headlessbuild, org.eclipse.e4.ui.workbench.swt.E4Application, org.eclipse.e4.ui.workbench.swt.GenTopic, org.eclipse.equinox.app.error, org.eclipse.equinox.p2.director, org.eclipse.equinox.p2.garbagecollector.application, org.eclipse.equinox.p2.publisher.InstallPublisher, org.eclipse.equinox.p2.publisher.EclipseGenerator, org.eclipse.equinox.p2.publisher.ProductPublisher, org.eclipse.equinox.p2.publisher.FeaturesAndBundlesPublisher, org.eclipse.equinox.p2.reconciler.application, org.eclipse.equinox.p2.repository.repo2runnable, org.eclipse.equinox.p2.repository.metadataverifier, org.eclipse.equinox.p2.artifact.repository.mirrorApplication, org.eclipse.equinox.p2.metadata.repository.mirrorApplication, org.eclipse.equinox.p2.touchpoint.natives.nativePackageExtractor, org.eclipse.equinox.p2.updatesite.UpdateSitePublisher, org.eclipse.equinox.p2.publisher.UpdateSitePublisher, org.eclipse.equinox.p2.publisher.CategoryPublisher, org.eclipse.help.base.infocenterApplication, org.eclipse.help.base.helpApplication, org.eclipse.help.base.indexTool, org.eclipse.ui.ide.workbench, com.ti.ccstudio.p2app, com.ti.common.core.initialize.
at org.eclipse.equinox.internal.app.EclipseAppContainer.startDefaultApp(EclipseAppContainer.java:248)
at org.eclipse.equinox.internal.app.MainApplicationLauncher.run(MainApplicationLauncher.java:29)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:388)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:243)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:656)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:592)
at org.eclipse.equinox.launcher.Main.run(Main.java:1498)
at org.eclipse.equinox.launcher.Main.main(Main.java:1471)
What am I missing?