This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AM5718: Debug MLO/U-Boot in CCS

Part Number: AM5718

Tool/software: Code Composer Studio

Hi,

I am using AM5718 IDK EVM,and ti-processor-sdk-linux-am57xx-evm-05.03.00.07.

I am trying to debug MLO and U-Boot using CCS Version: 8.3.0.00009.


I have followed
.

 

I am getting the message:

Can't find a source file at "arch/arm/lib/vectors.S"
Locate the file or edit the source lookup path to include its location.

When trying to put a hardware breakpoint, I get the following message:

No code is associated with "...... start.S", line 89 in any loaded symbols.

From the post in e2e.ti.com/.../87658
I understand that "Full symbolic debug ((--symdebug:dwarf, -g) needs to be enabled. I can find this option in CCS installed in windows PCs.
But can anyone tell me how to do this in CCS Version: 8.3.0.00009 installed in my Ubuntu PC ?

regards,

Anupama