This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/UCD3138PFCEVM-026: PWR026_PFC

Part Number: UCD3138PFCEVM-026


Tool/software: Code Composer Studio

in the following codes,What do 127  (#213)and 0x3ff(#449)mean ?

And  how to get them ?

  • The 127 is a number to see if the positive cycle has gone on for two long, Each count represents 100 usec, so 127 would be 12.7 milliseconds.  Even at 50 Hz, it should not be positive more than 10 milliseconds.  So in that case, we try to do something to make the code work for DC.  I don't think we have actually tested it at DC, however.

    The 3ff is the full range of the EADC DAC, so we are preventing a value outside the full range by clamping it to that level.  

  • Thanks for your help!