This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640R2F: Error -1170 and Error -2064 while programming the custom board.

Part Number: CC2640R2F
Other Parts Discussed in Thread: UNIFLASH,

Tool/software: Code Composer Studio

I am trying to program a custom board based on launchpad design.

I assembled the hardware and it is getting detected in the Flash Programmer.

However whenever I try to debug it using CCS, I get following errors:

Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.3.0.00003)
Cortex_M3_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.3.0.00003)

I checked following things:

1) VDDS, VDDR, DCDC voltages are in expected voltage range

2) Reset pin is pulled high and I observed it on oscilloscope for possibility of repeated resets. This seems not to be the case.

3) Mass erase uniflash or flash programmer is successful. However after this I still get the same error.

4) Tried changing cJTag frequency till 100 kHz (minimum value), this does not make any difference.

I have attached schematic for the reference.